Skip to main content
SRaic.1
Associate
May 16, 2023
Question

LCD not interpreting colors correctly using LTDC connected to STM32MP157F based custom board.

  • May 16, 2023
  • 0 replies
  • 914 views

We have a custom board based on STM32MP157 MPU and running AOSP, with AUO G101EVN010 LCD-TFT panel using an LVDS to LTDC converter for interface.

Setup of the system is done using the STM32MP1 distribution for Android.

I am able to get the panel to display the Android UI, but the issue is the colors on the UI.

Below is an image of the Android home screen:


_legacyfs_online_stmicro_images_0693W00000bkDBHQA2.pngObservation: RGB appears to be BRG.

When I pull down the notification panel from the top, the notification overlay shows and it is observed that colors in the background appear correct as seen below:


_legacyfs_online_stmicro_images_0693W00000bkDDDQA2.png 

Not getting where the issue is.

Using the MEDIA_BUS_FMT_RGB666_1X18 format for DRM and LTDC DT node settings as follows:

&ltdc {

  /* compatible = "simple-panel"; */

  status = "okay";

  bits-per-pixel = <16>;

  bus-width = <18>;

  display-timings {

    timing {

      clock-frequency = <68930000>;

      hactive = <1280>;

      vactive = <800>;

      hfront-porch = <120>;

      hback-porch = <0>;

      hsync-len = <8>;

      vback-porch = <10>;

      vfront-porch = <0>;

      vsync-len = <6>;

      hsync-active = <1>;

      vsync-active = <1>;

      de-active = <1>;

      pixelclk-active = <0>;

    };

  };

};

Can someone help out!

This topic has been closed for replies.