Associate III
April 15, 2025
Question
Many testcases are failed in TEE test application
- April 15, 2025
- 1 reply
- 359 views
I am working with openSTLinux as below:
- oe-manifest: TAG openstlinux-6.6-yocto-scarthgap-mpu-v25.03.19
- Hardware: STM32MP257F-DK
- Image: st-image-weston
- Secure boot is enable and device is closed (BSEC_STATE_SEC_CLOSED)
- Remove Debug Support in Linux Device tree as KYAO suggested in this topic
I ran command xtest. The command is provides by a recipe optee-test_4.0.bb in meta-st-openstlinux. I found that many test cases are failed. They are related to pcks11. I attached the log file while running xtest.
28179 subtests of which 33 failed
134 test cases of which 29 failed
0 test cases were skipped
TEE test application done!Is there any problem with OPTEE OS? Please help me solve the problem or give suggestions to solve this problem.