Skip to main content
Visitor II
June 19, 2023
Question

OpenSTLinux SDK Manager can't find updated SDK

  • June 19, 2023
  • 1 reply
  • 1078 views

Hi 

I have used the "bitbake -c populate_sdk st-image-weston" command to generate an updated SDK with OpenCV and ZerMQ packages. The SDK is generated successfully.

The issue is when I want to use this SDK in STM32CubeIDE, since I can't seem to find the SDK in "OpenSTLinux SDK Manager" under Window ==> Preferences. The manager can easily find the standard SDK which can be downloaded from the website. 

I suspect the issue to be the version name, since the updated SDK outputs "4.0.4-snapshot" instead of "4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23" when entering:

PC >> echo $OECORE_SDK_VERSION

What can I do to fix this? :)

(OpenSTLinux SDK Manager unable to see SDK)

MarcusRJ_0-1687161319965.png

(Updated SDK folder)

MarcusRJ_1-1687161359883.png

 

 

This topic has been closed for replies.

1 reply

Olivier GALLIEN
Technical Moderator
June 29, 2023

Hi @MarcusRJ ,

 

In order to be seen by "SDK manager"  SDK version might contain "openstlinux-" 

 

 

Hope it help 

 

Olivier 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.