OTP Bits Cannnot read
- February 22, 2024
- 3 replies
- 2657 views
Hi All.
I use discovery board of STM32MP157F-DK2 .
So I want t to try read OTP Bits via STM32CubeProgrammer , But I find 2 errs.
The err things search ST Community, I fund it.
Can't read OTP bits on STM32MP157C-DK2 using STM32CubeProgrammer
So I Try to refer Answer,I can't know where wrong.
(I reload Flashlayout for OTP exposing )
Sorry for my poor English,Thinks at all.
/********************************************************************************************************************/
u6326@Prodisk:~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin$ ./STM32_Programmer_CLI -c port=usb1 -d FlashLayout.tsv -otp displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
SN : 003200433132511831373339
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP157FAC Rev.Z
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
Flashing service completed successfully
UPLOADING OTP STRUCTURE ...
Partition : 0xF2
Size : 1024 Bytes
Uploading OTP data:
Error: Read OTP Partition failed
Error: Uploading the OTP structure failed
Error: Initializing the OTP structure failed
/********************************************************************************************************************/