Associate II
March 10, 2023
Solved
Problem to flashing immage to STM32MPF-DK2
- March 10, 2023
- 5 replies
- 5393 views
I cannot load the image into the SD card of the STM32MP157F-DK2 board.
I set the switches to OFF
I start the board that starts in BOOT FOR FLASCHING (only the LD4 led is on steady red)
Through the terminal or graphical STMProgrammer I start the download of the image (file: FlashLayout_sdcard_stm32mp157f-dk2-trusted.tsv)
It loads Partition ID 0x001 correctly, finishes loading Partition ID 0x003, then the board exits the BOOT FOR FLASHING mode (the blue LD8 LED lights up and the LD6 LED flashes red) and the software returns to me Reconnecting the device ...