Skip to main content
Associate
March 4, 2025
Solved

Qt Rotation Issue on STM32MP157C with LTDC Display Controller

  • March 4, 2025
  • 3 replies
  • 1275 views

Issue Summary

When trying to rotate the display on an STM32MP157C board from landscape (800x480) to portrait (480x800) mode, I'm experiencing issues. Using the /sys/class/graphics/fb0/rotate interface doesn't actually rotate the display, and using Qt's EGLFS with rotation settings results in only half the screen being rotated properly.

Hardware Information

  • Board: STM32MP157C
  • Display controller: STM32 LTDC (LCD-TFT Display Controller)
  • Screen dimensions: 800x480 (native landscape)
  • Framebuffer: /dev/fb0
  • DRM device: /dev/dri/card0

What I've Tried

  1. Setting framebuffer rotation via sysfs: echo 1 > /sys/class/graphics/fb0/rotate

This changes the value but doesn't affect display.

Using EGLFS KMS config with rotation:

QString configPath = "/tmp/eglfs_kms.json";
QFile configFile(configPath);
if (configFile.open(QIODevice::WriteOnly | QIODevice::Text)) {
configFile.write("{\n"
" \"device\": \"/dev/dri/card0\",\n"
" \"outputs\": [\n"
" {\n"
" \"name\": \"DPI-1\",\n"
" \"mode\": \"480x800\",\n"
" \"transform\": \"rotate-90\"\n"
" }\n"
" ]\n"
"}\n");
configFile.close();
qputenv("QT_QPA_EGLFS_KMS_CONFIG", configPath.toUtf8());
}

This partially works (screen reports correct orientation) but only half the screen is correctly rotated.

3.QML-based rotation:

Item {
width: parent.height
height: parent.width
anchors.centerIn: parent
rotation: 90
transformOrigin: Item.Center
// Content goes here
}

This somewhat works , but i dont this this is a proper solution

4.Setting various environment variables:

QT_QPA_EGLFS_ROTATION=90
QSG_RENDER_LOOP=basic

 

5.I tried different variations of the EGLFS configuration, including:

{
"device": "/dev/dri/card0",
"hwcursor": false,
"outputs": [
{
"name": "DPI-1",
"mode": "800x480",
"transform": "rotate-90"
}
]
}

And:

{
"device": "/dev/dri/card0",
"hwcursor": false,
"gbm": true,
"outputs": [
{
"name": "DPI-1",
"format": "xrgb8888",
"rotation": 90
}
]
}

6.Checked the device tree, which shows:

display-controller@5a001000 {
compatible = "st,stm32-ltdc";
reg = <0x5a001000 0x400>;
interrupts = <0x00 0x58 0x04 0x00 0x59 0x04>;
clocks = <0x0e 0xa7>;
clock-names = "lcd";
resets = <0x0e 0xc00>;
status = "okay";
/* No rotation property here */
}

 

7.Used modetest to inspect DRM properties:

The output shows mode support for 800x480 but no explicit rotation property.

 

Debug Information

From my debugging logs, when using the EGLFS configuration, Qt correctly reports the screen orientation as portrait:

=== SCREEN INFORMATION ===
Screen size: QSize(480, 800)
Physical size (mm): QSizeF(86, 154)
Platform: "eglfs"
Orientation: Qt::PortraitOrientation

 

However, visually, only half the screen appears correctly rotated. The debug logs show that the EGLFS configuration is being loaded correctly:

 

qt.qpa.eglfs.kms: Loading KMS setup from "/tmp/eglfs_kms.json"
qt.qpa.eglfs.kms: Adding QPlatformScreen 0x816d0 ( "UNKNOWN1" ) to QPA with geometry QRect(0,0 480x800)

When examining the available planes with modetest, I see:

qt.qpa.eglfs.kms: Loading KMS setup from "/tmp/eglfs_kms.json"
qt.qpa.eglfs.kms: Adding QPlatformScreen 0x816d0 ( "UNKNOWN1" ) to QPA with geometry QRect(0,0 480x800)

 

Currently, I'm using a QML-based rotation approach, but it causes performance issues with animations and effects. I'm looking for a proper hardware-accelerated rotation solution that works with the STM32 LTDC controller.

 

Question

How can I get proper full-screen rotation with the STM32 LTDC controller? Is there a specific driver setting or Qt configuration I'm missing? Are there known limitations with this hardware?

Best answer by lepot
#ifndef SCREENORIENTATIONHANDLER_H
#define SCREENORIENTATIONHANDLER_H

#include <QObject>
#include <QQuickWindow>

/**
 * @brief The ScreenOrientationHandler class allows dynamic rotation handling
 * for QML content on embedded STM32 platforms using the LTDC display controller.
 */
class ScreenOrientationHandler : public QObject
{
 Q_OBJECT
 Q_PROPERTY(int screenRotation READ screenRotation WRITE setScreenRotation NOTIFY screenRotationChanged)

public:
 explicit ScreenOrientationHandler(QObject *parent = nullptr);

 int screenRotation() const { return m_rotation; }
 void setScreenRotation(int rotation);

 // Should be called from main.cpp after QGuiApplication is created
 Q_INVOKABLE void initialize();

 // Attach to a specific QQuickWindow to manage its rotation
 Q_INVOKABLE void attachToWindow(QQuickWindow *window);

signals:
 void screenRotationChanged();

private slots:
 void handleFocusWindowChanged(QWindow *window);

private:
 void applyRotation();

 int m_rotation = 0;
 QQuickWindow *m_window = nullptr;
};

#endif // SCREENORIENTATIONHANDLER_H
#include "ScreenOrientationHandler.h"
#include <QGuiApplication>
#include <QScreen>
#include <QQuickItem>

ScreenOrientationHandler::ScreenOrientationHandler(QObject *parent)
 : QObject(parent)
{
}

void ScreenOrientationHandler::setScreenRotation(int rotation)
{
 rotation = rotation % 360;
 if (rotation < 0) rotation += 360;

 if (m_rotation != rotation) {
 m_rotation = rotation;
 applyRotation();
 emit screenRotationChanged();
 }
}

void ScreenOrientationHandler::initialize()
{
 applyRotation();

 if (QGuiApplication *app = qobject_cast<QGuiApplication*>(QGuiApplication::instance())) {
 connect(app, &QGuiApplication::focusWindowChanged,
 this, &ScreenOrientationHandler::handleFocusWindowChanged);
 }
}

void ScreenOrientationHandler::handleFocusWindowChanged(QWindow *window)
{
 if (auto *qWindow = qobject_cast<QQuickWindow *>(window)) {
 attachToWindow(qWindow);
 }
}

void ScreenOrientationHandler::attachToWindow(QQuickWindow *window)
{
 if (m_window != window) {
 m_window = window;

 if (m_window) {
 applyRotation();

 connect(m_window, &QQuickWindow::widthChanged, this, &ScreenOrientationHandler::applyRotation);
 connect(m_window, &QQuickWindow::heightChanged, this, &ScreenOrientationHandler::applyRotation);
 }
 }
}

void ScreenOrientationHandler::applyRotation()
{
 if (!m_window) return;

 QQuickItem *rootItem = m_window->contentItem();
 if (!rootItem) return;

 rootItem->setProperty("rotation", m_rotation);

 if (m_rotation == 90 || m_rotation == 270) {
 rootItem->setProperty("clip", true); // Prevent rendering artifacts

 rootItem->setWidth(m_window->height());
 rootItem->setHeight(m_window->width());
 rootItem->setX((m_window->width() - m_window->height()) / 2);
 rootItem->setY((m_window->height() - m_window->width()) / 2);
 } else {
 rootItem->setWidth(m_window->width());
 rootItem->setHeight(m_window->height());
 rootItem->setX(0);
 rootItem->setY(0);
 }
}
#include <QGuiApplication>
#include <QQmlApplicationEngine>
#include <QQmlContext>
#include <QQuickWindow>
#include <QCursor>

#include "ScreenOrientationHandler.h" // renamed handler for clarity

int main(int argc, char *argv[])
{
 QCoreApplication::setAttribute(Qt::AA_EnableHighDpiScaling);

 // Hide mouse cursor (optional)
 QGuiApplication app(argc, argv);
 QGuiApplication::setOverrideCursor(QCursor(Qt::BlankCursor));

 // Setup rotation
 ScreenOrientationHandler orientationHandler;
 orientationHandler.setScreenRotation(90); // Portrait mode

 // QML engine setup
 QQmlApplicationEngine engine;
 const QUrl mainQmlUrl(QStringLiteral("qrc:/qml/main.qml"));

 // Attach rotation handler to the QML window once it's created
 QObject::connect(&engine, &QQmlApplicationEngine::objectCreated,
 &app,
 [mainQmlUrl, &orientationHandler](QObject *obj, const QUrl &objUrl)
 {
 if (!obj && objUrl == mainQmlUrl)
 QCoreApplication::exit(-1);

 if (auto *win = qobject_cast<QQuickWindow *>(obj))
 orientationHandler.attachToWindow(win);
 }, Qt::QueuedConnection);

 engine.load(mainQmlUrl);
 return app.exec();
}

Here is the full implementation with how to use it in main.c 

From here you just define you windows in designer 480x800 for example and you can design properly and run properly in portrait mode for embeded devices.

IF you have any suggestions or improvements of this code please share your thoughts , because from what i saw a lot of people have this problem.

 

#QT PORTATI MODE QML

3 replies

Erwan SZYMANSKI
Technical Moderator
March 5, 2025

Hello @lepot ,
On STM32MP15X, LTDC has no rotation option that can be done in HW.
From my previous tests, I think the best balance between rendering and performances using QML was to have a global container (QML Rect or Item) under the QML main Window applying the rotation.

I put you an example of an old demo I had on this platform (main.qml):

 

ApplicationWindow {
 id: base
 width: _windowWidth
 height: _windowHeight
 visible: true

 Item {
 anchors.centerIn: base.contentItem
 width: _portrait ? base.height : base.width
 height: _portrait ? base.width : base.height
 rotation: _portrait ? 90 : 0

 <.... app ....>
 }
}

 

I hope it will help you go forward.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
May 27, 2025

I'm trying this on Qt 6.9. Rotating the whole application this way seems to work, however any Popup based QML items (Menu, ComboBox drop down, ...) are not rotated, because they are parented to the window overlay.

You need to rotate the overlay as well:

Overlay.overlay.rotation: _portrait ? 90 : 0

 

lepotAuthor
Associate
June 8, 2025

@Erwan SZYMANSKI , @wincak Thank you for you suggestons , it worked , soon i will provide the whole implementation , where ytou could choose different rotations , and it is only defined once in the main.c

lepotAuthorBest answer
Associate
June 8, 2025
#ifndef SCREENORIENTATIONHANDLER_H
#define SCREENORIENTATIONHANDLER_H

#include <QObject>
#include <QQuickWindow>

/**
 * @brief The ScreenOrientationHandler class allows dynamic rotation handling
 * for QML content on embedded STM32 platforms using the LTDC display controller.
 */
class ScreenOrientationHandler : public QObject
{
 Q_OBJECT
 Q_PROPERTY(int screenRotation READ screenRotation WRITE setScreenRotation NOTIFY screenRotationChanged)

public:
 explicit ScreenOrientationHandler(QObject *parent = nullptr);

 int screenRotation() const { return m_rotation; }
 void setScreenRotation(int rotation);

 // Should be called from main.cpp after QGuiApplication is created
 Q_INVOKABLE void initialize();

 // Attach to a specific QQuickWindow to manage its rotation
 Q_INVOKABLE void attachToWindow(QQuickWindow *window);

signals:
 void screenRotationChanged();

private slots:
 void handleFocusWindowChanged(QWindow *window);

private:
 void applyRotation();

 int m_rotation = 0;
 QQuickWindow *m_window = nullptr;
};

#endif // SCREENORIENTATIONHANDLER_H
#include "ScreenOrientationHandler.h"
#include <QGuiApplication>
#include <QScreen>
#include <QQuickItem>

ScreenOrientationHandler::ScreenOrientationHandler(QObject *parent)
 : QObject(parent)
{
}

void ScreenOrientationHandler::setScreenRotation(int rotation)
{
 rotation = rotation % 360;
 if (rotation < 0) rotation += 360;

 if (m_rotation != rotation) {
 m_rotation = rotation;
 applyRotation();
 emit screenRotationChanged();
 }
}

void ScreenOrientationHandler::initialize()
{
 applyRotation();

 if (QGuiApplication *app = qobject_cast<QGuiApplication*>(QGuiApplication::instance())) {
 connect(app, &QGuiApplication::focusWindowChanged,
 this, &ScreenOrientationHandler::handleFocusWindowChanged);
 }
}

void ScreenOrientationHandler::handleFocusWindowChanged(QWindow *window)
{
 if (auto *qWindow = qobject_cast<QQuickWindow *>(window)) {
 attachToWindow(qWindow);
 }
}

void ScreenOrientationHandler::attachToWindow(QQuickWindow *window)
{
 if (m_window != window) {
 m_window = window;

 if (m_window) {
 applyRotation();

 connect(m_window, &QQuickWindow::widthChanged, this, &ScreenOrientationHandler::applyRotation);
 connect(m_window, &QQuickWindow::heightChanged, this, &ScreenOrientationHandler::applyRotation);
 }
 }
}

void ScreenOrientationHandler::applyRotation()
{
 if (!m_window) return;

 QQuickItem *rootItem = m_window->contentItem();
 if (!rootItem) return;

 rootItem->setProperty("rotation", m_rotation);

 if (m_rotation == 90 || m_rotation == 270) {
 rootItem->setProperty("clip", true); // Prevent rendering artifacts

 rootItem->setWidth(m_window->height());
 rootItem->setHeight(m_window->width());
 rootItem->setX((m_window->width() - m_window->height()) / 2);
 rootItem->setY((m_window->height() - m_window->width()) / 2);
 } else {
 rootItem->setWidth(m_window->width());
 rootItem->setHeight(m_window->height());
 rootItem->setX(0);
 rootItem->setY(0);
 }
}
#include <QGuiApplication>
#include <QQmlApplicationEngine>
#include <QQmlContext>
#include <QQuickWindow>
#include <QCursor>

#include "ScreenOrientationHandler.h" // renamed handler for clarity

int main(int argc, char *argv[])
{
 QCoreApplication::setAttribute(Qt::AA_EnableHighDpiScaling);

 // Hide mouse cursor (optional)
 QGuiApplication app(argc, argv);
 QGuiApplication::setOverrideCursor(QCursor(Qt::BlankCursor));

 // Setup rotation
 ScreenOrientationHandler orientationHandler;
 orientationHandler.setScreenRotation(90); // Portrait mode

 // QML engine setup
 QQmlApplicationEngine engine;
 const QUrl mainQmlUrl(QStringLiteral("qrc:/qml/main.qml"));

 // Attach rotation handler to the QML window once it's created
 QObject::connect(&engine, &QQmlApplicationEngine::objectCreated,
 &app,
 [mainQmlUrl, &orientationHandler](QObject *obj, const QUrl &objUrl)
 {
 if (!obj && objUrl == mainQmlUrl)
 QCoreApplication::exit(-1);

 if (auto *win = qobject_cast<QQuickWindow *>(obj))
 orientationHandler.attachToWindow(win);
 }, Qt::QueuedConnection);

 engine.load(mainQmlUrl);
 return app.exec();
}

Here is the full implementation with how to use it in main.c 

From here you just define you windows in designer 480x800 for example and you can design properly and run properly in portrait mode for embeded devices.

IF you have any suggestions or improvements of this code please share your thoughts , because from what i saw a lot of people have this problem.

 

#QT PORTATI MODE QML