Skip to main content
Visitor II
March 25, 2026
Question

Request for IBIS model for STM32MP157CAC3 DDR + high-speed IO (DDR, SDMMC, Ethernet)

  • March 25, 2026
  • 1 reply
  • 92 views

Dear ST Community,
I am currently working on a custom hardware design based on the STM32MP157CAC3 MPU, which includes LPDDR3 memory (Micron MT52L256M32D1PF) and multiple high-speed interfaces.
As part of my signal integrity and high-speed design validation process, I need simulation models to conduct accurate analysis.
I want to request the following:

IBIS models for STM32MP157CAC3, specifically covering:

1. DDR interface (LPDDR2/LPDDR3 controller)

2. SDMMC interface

3. Any other relevant high-speed I/Os(MIPI, LTDC, DCMI, SDMMC)

S-parameter models (if available) for:

1. High-speed I/O buffers

2. DDR interface pins or PHY

Any additional resources that may support SI/PI analysis, such as:

1. IBIS-AMI models (if available)

2. Reference simulation setups

3. Application notes related to DDR signal integrity

Project details:

Custom PCB (not a direct copy of STM32MP1 DK2)

LPDDR3 operating btw 300 - 800 MHz

Goal: Pre-layout and post-layout SI validation (HyperLynx/ADS

I understand that some of these models may require NDA access. I am willing to follow the necessary process if required.

Please let me know the appropriate steps to obtain these files.

1 reply

PatrickF
Technical Moderator
March 25, 2026
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here