Skip to main content
Associate II
November 8, 2024
Solved

Secure boot TF-A error - BL2: Failed to load image id 1 (-80) : STM32MP2

  • November 8, 2024
  • 1 reply
  • 1622 views

Hi,

I am trying to boot a signed TF-A image on my STM32m257f compiled with TRUSTED_BOARD_BOOT support (Compiled in f-a-stm32mp.inc recipe from meta-st-stm32mp, mickledore branche).

When the board is powered up, i got this error:

 

 

NOTICE: CPU: STM32MP257FAI Rev.B
NOTICE: Model: STMicroelectronics STM32MP257F-EV1 Evaluation Board
NOTICE: Board: MB1936 Var1.0 Rev.C-01
NOTICE: BL2: v2.8-stm32mp2-r2.0(release):lts-v2.8.15-dirty(567af710)
NOTICE: BL2: Built : 00:51:33, Jan 26 2024
NOTICE: TRUSTED_BOARD_BOOT support enabled
ERROR: BL2: Failed to load image id 1 (-80)

 

 

 

I've already fuse my PKHTH with the stm32key command and my binary is signed with the right key. The board boots normally when I install a TF-A binary without TRUSTED_BOARD_BOOT support.

Do you have any idea please?

Thanks

Best answer by zakariazh

After a debug session, the problem is coming when the TF-A tries to check the hash of the fip containing the OPTEE and bootloader.

It was an error when calling cert_create tool with an empty password argument when using a private key without password. If you face this error, make sure to remove this argument if no password if used.


Thank you

1 reply

zakariazhAuthorBest answer
Associate II
November 10, 2024

After a debug session, the problem is coming when the TF-A tries to check the hash of the fip containing the OPTEE and bootloader.

It was an error when calling cert_create tool with an empty password argument when using a private key without password. If you face this error, make sure to remove this argument if no password if used.


Thank you