Senior
February 13, 2022
Question
STM32MP1 boot stuck on SP_MIN: Preparing exit to normal world
- February 13, 2022
- 3 replies
- 1903 views
After buildroot I'm trying to get the yocto build to work. I'm using openstlinux-5.10-dunfell-mp1-21-11-17. The boot process always stops on SP_MIN: Preparing exit to normal world. Yes, I have already read the https://st.force.com/community/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide. I do have the memory correct and I do not have any pins configured in &rcc. The same device tree file(s) works on buildroot. How can I debug this? The board I'm using is from MYiR (MYD-YA157C).
Edit: I'm using custom machine, which is defined in layers/meta-st/meta-st-stm32mp-addons/conf/machine