STM32MP1 ethernet issue
- July 16, 2024
- 3 replies
- 4283 views
Hi,
We are using the STM32MP157CAA3 SoC in our design and are having some Ethernet issues:
As we had problems sourcing the Realtek PHY from the reference design we use the microchip LAN8830T-V/PSA Ethernet PHY which should support Gigabit Ethernet.
When setting booting the device and connecting an Ethernet cable we observe the following issue:
1. With 10 MBit or router, the device probes and from both U-boot and Linux we can do dhcp request. But we never get an answer (no IP etc).
2. With 100 MBit or 1000 MBit speed, the linux kernel throws a panic after some time related to DMA (sometimes also the probing fails for the DMA engine).
Both paths never show any data coming through the Ethernet port: (DCHP requests seem to be unanswered (don't arrive on server side) and ping also doesn't arrive. LED's remain stale (green = constant ON, orange LED = off).
Bootlog during success:
root@board:~# dmesg | grep eth
[ 0.000000] psci: probing for conduit method from DT.
[ 0.269703] usbcore: registered new interface driver cdc_ether
[ 0.289476] optee: probing for conduit method.
[ 1.633140] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found
[ 1.638473] stm32-dwmac 5800a000.ethernet: no regulator found
[ 1.638983] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[ 1.644693] stm32-dwmac 5800a000.ethernet: DWMAC4/5
[ 1.649759] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[ 1.656999] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[ 1.664289] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[ 1.671191] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[ 1.677637] stm32-dwmac 5800a000.ethernet: TSO supported
[ 1.682709] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.690628] stm32-dwmac 5800a000.ethernet: Enabled L3L4 Flow TC (entries=2)
[ 1.697535] stm32-dwmac 5800a000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.704522] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[ 1.710332] stm32-dwmac 5800a000.ethernet: Using 32/32 bits DMA host/device width
[ 4.623237] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 4.631424] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 4.644235] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 4.651974] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 4.660496] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 4.668620] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 8.880230] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 10Mbps/Full - flow control rx/tx
[ 8.887340] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Bootlog during failure:
root@wesl:~# dmesg | grep eth
[ 0.000000] psci: probing for conduit method from DT.
[ 0.269963] usbcore: registered new interface driver cdc_ether
[ 0.289696] optee: probing for conduit method.
[ 1.633444] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found
[ 1.638790] stm32-dwmac 5800a000.ethernet: no regulator found
[ 1.639302] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[ 1.645012] stm32-dwmac 5800a000.ethernet: DWMAC4/5
[ 1.650074] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[ 1.657319] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[ 1.664610] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[ 1.671509] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[ 1.677850] stm32-dwmac 5800a000.ethernet: TSO supported
[ 1.683023] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.690841] stm32-dwmac 5800a000.ethernet: Enabled L3L4 Flow TC (entries=2)
[ 1.697848] stm32-dwmac 5800a000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.704736] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[ 1.710643] stm32-dwmac 5800a000.ethernet: Using 32/32 bits DMA host/device width
[ 4.976410] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 4.985026] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 5.997554] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[ 6.002358] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 6.011322] stm32-dwmac 5800a000.ethernet eth0: __stmmac_open: Hw setup failed
[ 9.224884] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 9.241514] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 9.254347] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 9.262215] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 9.271172] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 9.278538] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 13.439784] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 13.446896] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 19.687950] NETDEV WATCHDOG: eth0 (stm32-dwmac): transmit queue 0 timed out
[ 19.839844] stm32-dwmac 5800a000.ethernet eth0: Reset adapter.
[ 19.855494] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 19.863823] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 19.876709] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 19.884033] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 19.892921] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 19.898791] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 24.079787] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 24.086899] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Panic:
[ 19.676490] ------------[ cut here ]------------
[ 19.679713] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:525 dev_watchdog+0x208/0x27c
[ 19.687950] NETDEV WATCHDOG: eth0 (stm32-dwmac): transmit queue 0 timed out
[ 19.694933] Modules linked in:
[ 19.697987] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 6.1.28 #1
[ 19.703864] Hardware name: STM32 (Device Tree Support)
[ 19.709041] unwind_backtrace from show_stack+0x10/0x14
[ 19.714232] show_stack from dump_stack_lvl+0x40/0x4c
[ 19.719318] dump_stack_lvl from __warn+0x78/0x158
[ 19.724102] __warn from warn_slowpath_fmt+0x148/0x1c0
[ 19.729187] warn_slowpath_fmt from dev_watchdog+0x208/0x27c
[ 19.734882] dev_watchdog from call_timer_fn+0x34/0x1a8
[ 19.740079] call_timer_fn from __run_timers+0x274/0x378
[ 19.745370] __run_timers from run_timer_softirq+0x2c/0x40
[ 19.750863] run_timer_softirq from __do_softirq+0x138/0x408
[ 19.756555] __do_softirq from __irq_exit_rcu+0xc0/0x10c
[ 19.761837] __irq_exit_rcu from irq_exit+0x8/0x10
[ 19.766609] irq_exit from __irq_svc+0x88/0xc8
[ 19.771077] Exception stack(0xc1201ee8 to 0xc1201f30)
[ 19.776048] 1ee0: 00000000 00000000 0001c359 c0119740 00000000 c1208f40
[ 19.784247] 1f00: c1324320 c1208f40 00000000 00000000 10c5387d 00000000 7fffffff c1201f38
[ 19.792441] 1f20: c0109080 c0109084 60030013 ffffffff
[ 19.797504] __irq_svc from arch_cpu_idle+0x38/0x3c
[ 19.802287] arch_cpu_idle from default_idle_call+0x40/0x12c
[ 19.807977] default_idle_call from cpuidle_idle_call+0x18c/0x1ec
[ 19.814067] cpuidle_idle_call from do_idle+0x94/0xc8
[ 19.819145] do_idle from cpu_startup_entry+0x18/0x1c
[ 19.824122] cpu_startup_entry from rest_init+0xd0/0xd4
[ 19.829406] rest_init from arch_post_acpi_subsys_init+0x0/0x8
[ 19.835205] ---[ end trace 0000000000000000 ]---
[ 19.839844] stm32-dwmac 5800a000.ethernet eth0: Reset adapter.
[ 19.855494] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 19.863823] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 19.871457] dwmac4: Master AXI performs any burst length
[ 19.876709] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
We have the idea that it is clock-tree related (See attached) .
The design is strapped so the PHY generates the clock-source (125MHz for 1GBit)
Some matching issues that we searched on the forum:
- https://community.st.com/t5/stm32-mpus-embedded-software/stm32mp157-ethernet-problem/td-p/280709 pointed us to check the strapping to have the clock generated by the PHY
Relevant part of our schematics:
Our OPtee/tf-a rcc config see attached dts files (actually dtsi files, but not allowed).
both are included by dts file like:
/dts-v1/;
#include "stm32mp157.dtsi"
#include "stm32mp15xc.dtsi"
#include "stm32mp15-pinctrl.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15xx-<ourBoard>-common.dtsi" //<-- the attached files
/ {
model = "proto 0 board";
compatible = "st,stm32mp157c-dk2", "st,stm32mp157";
chosen {
stdout-path = "serial0:115200n8";
};
};
Clocks measured:
Xtal connected to PHY = 25Mhz,
Clock output from PHCLK125= 125Mhz,
RX Clock frequency = 25Mhz,
TX Clock frequency = 2,5Mhz. [Why different compared to RX?]
We have some design length differences in signals from Ethernet controller to PHY, which are a in pico second range and should be within limit of the PHY:

Signal length of lines & calculated delays
| Name | Signal Length (mm) | Delay (ps) |
| ETH1_GTX_CLK_PP1 | 133 | 910 |
| ETH1_MDC_PP1 | 144 | 990 |
| ETH1_MDIO_PP1 | 153 | 1052 |
| ETH1_RXD0-NetR1003_2_PP1 | 137 | 935 |
| ETH1_RXD1-NetR1002_2_PP1 | 143 | 974 |
| ETH1_RXD2-NetR1001_2_PP1 | 121 | 799 |
| ETH1_RXD3-NetR1000_2_PP1 | 162 | 1110 |
| ETH1_RX_CLK-NetR1004_2_PP1 | 160 | 1098 |
| ETH1_RX_CTL-NetR1005_2_PP1 | 126 | 833 |
| ETH1_TXD0_PP1 | 188 | 1294 |
| ETH1_TXD1_PP1 | 155 | 1038 |
| ETH1_TXD2_PP1 | 181 | 1239 |
| ETH1_TXD3_PP1 | 205 | 1400 |
| ETH1_TX_CTL_PP1 | 121 | 808 |
| ETH_CLK125OUT-NetR1006_2_PP1 | 155 | 1058 |
| ETH_GPIO2-NetR1044_1_PP1 | 203 | 1407 |
| ETH_GPIO3-NetR1037_1_PP1 | 169 | 1163 |
| ETH_GPIO4-NetR1038_1_PP1 | 160 | 1101 |
| ETH_GPIO5-NetR1039_1_PP1 | 131 | 867 |
| ETH_RESET_N-NetC1033_2_PP1 | 144 | 982 |