Associate II
January 22, 2024
Solved
STM32MP135F - How to enable ETH2 using MII to connect Switch
- January 22, 2024
- 2 replies
- 3103 views
We have designed 2 seperate boards, main board has STM32MP135FAE on board connected to Microchip LAN8742 via ethernet1 mac and it is working. second board is a network board and has Marvell 88E6185 switch on board. Ethernet2 mac on STM32MP135F is connected to Port9 at the Switch using MII. However, STM32MP135F is not enabling internal clock. And eth2 is not activated.
- I have tried setting ETH clock at 25MHz, no luck.
I have attached my configuration files and clock settings and dmesg log.
Any idea what might be wrong on my configurations?