Skip to main content
Associate
October 3, 2024
Question

stm32mp157 apt-get install x-linux-ai-tool unable to locate

  • October 3, 2024
  • 1 reply
  • 834 views

I am a newcomer and not very good at using Linux. I hope to try running the model on the device. I am using a third-party development board. Is the tutorial on the official website applicable or can I use an API
Snipaste_2024-10-03_22-45-11.jpg

1 reply

PatrickF
Technical Moderator
October 4, 2024

Hi @wink 

according to prompt I see on your capture, not sure you are using an ST Board with openSTLinux Starter Package.

For OpenSTLinux Starter Package, please see https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_Tool

Did 'apt-get update' works ?

I'm not expert, but if needed, the following link should help to build X-LINUX-AI for your board.
see https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_Developer_package or https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_Distribution_package

Regards.

 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
winkAuthor
Associate
October 4, 2024

I am not using the openSTLinux Starter Package, I am using a third-party development board and I am concerned that flashing this package may not work properly. I am looking for other ways to call the librarySnipaste_2024-10-04_14-45-32.jpg

Jean-Marc B
ST Employee
October 4, 2024

Hi @wink 

the x-linux packages installers are provided through the «updates» component of the OpenSTLinux distribution. This component has to be built separately.

Details are given here:

https://github.com/stmicroelectronics/meta-st-pkgrepo-updates

Best regards,

--JM