Skip to main content
ALong.4
Associate II
May 19, 2023
Question

STM32MP157F: DMA support on USB/CRYPTO/eMMC

  • May 19, 2023
  • 0 replies
  • 778 views

Hi,

I am interested in using the STM32MP157F for the following tasks:

  1. Receiving data from USB 2.0.
  2. Encrypting the received data using AES 256.
  3. Storing the encrypted data in an external eMMC.
  4. Preferably utilizing DMA for efficient data transfers.

I would like to know if it is possible to configure DMA channels to enable direct peripheral-to-peripheral communication, such as USB 2.0 -> CRYPTO (AES 256) -> eMMC.

Additionally, it would be greatly appreciated if you could provide an example or reference on how to utilize DMA with USB, cryptographic operations, and eMMC.

Thank you.

Best regards,

Alessandro

This topic has been closed for replies.