STM32MP257F-EV1, no DFU detected by Cube
I am trying to connect the STM32MP257F-EV1, following the guide on the wiki. Followed the LInux preparation. At startup, I get a blinking RED LD1 and steady green LED
When start the laptop on windows, the device manager shows a DFU device a. But when booting up LInux, no device in DFU mode is detected by CubeProgrammer 2.210, either through the GUI or the CLI interface.
Having tried several possible workarounds—such as changing cables, reinstalling drivers and VMs, and reinstalling CubeProgrammer and the supporting software
The board seems to be working as when I reconfigure the boot switches, the display and camera work OK
Could someone suggest what I might be doing wrong or if there is a known solution?
Linux shows this:
T: Bus=01 Lev=01 Prnt=04 Port=02 Cnt=01 Dev#= 11 Spd=480 MxCh= 0
D: Ver= 2.00 Cls=00(>ifc ) Sub=00 Prot=00 MxPS=64 #Cfgs= 1
P: Vendor=0483 ProdID=df11 Rev=02.00
S: Manufacturer=STMicroelectronics
S: Product=DFU in HS Mode @Device ID /0x505, @Revision ID /0x2000
S: SerialNumber=004600244236500700333258
C: #Ifs= 1 Cfg#= 1 Atr=c0 MxPwr=100mA
I: If#= 0 Alt= 0 #EPs= 0 Cls=fe(app. ) Sub=01 Prot=02 Driver=(none)
Thanks a lot,
Javier