Skip to main content
Associate
August 26, 2025
Question

SXGMAC Ethernet Driver Query

  • August 26, 2025
  • 6 replies
  • 633 views

Hi

I am using Marvell Ethernet Phy(mv88q2220) in our project,i have integrated my Marvell driver into SDK and it is probing as well, we are using sxgmac driver for mac, while i am trying to initialize the eth0 interface i am facing issues related to validation of phy and phy is not able to attach.I have checked the phy-mode also it is configured correctly. I am attaching the error  logs also, Can anyone suggest what could the potential cause of this issue ?

Error Logs:

root@sadk:~# ifconfig eth0 192.168.10.1 up
SIOCSIFFLAGS: Invalid argument
SIOCSIFFLAGS: Invalid argument

Dmesg Logs:

[   55.096204] sxgmac 16cc8000.ethernet eth0: validation of  with support 00000000,00000000,00006000 and advertisement 00000000,00000000,00000000 failed: -EINVAL
[   55.096449] sxgmac 16cc8000.ethernet eth0: __stmmac_open: Cannot attach to PHY (error: -22)
[   55.364867] sxgmac 16cc8000.ethernet: is_dsp_running changed to true
[   55.365900] sxgmac 16cc8000.ethernet: MAC address filter register failure
[   55.684876] sxgmac 16cc8000.ethernet: is_dsp_running changed to false

 

Thanks & Regards

Uthaya

6 replies

GatienC
ST Employee
August 28, 2025

Hello,

I suspect it's related to the PHY state. Can you check that the PHY is powered correctly at that point. Have you given enough time for the PHY to initialize (should be specified in spec)? Try to add a delay at the end of its configuration.

 

Best regards,

Gatien

GatienC
ST Employee
August 28, 2025

Also, why are you using sxgmac?

UthayaAuthor
Associate
August 28, 2025

Hi GatienC

We are using sxgmac for mac driver(ethernet sub-controller, Synopsys IP Core),i have added a TXCLK internal delay for 1.3 ns and tried but i am facing the same issue.

GatienC
ST Employee
August 29, 2025

Hi,

 

What exactly is you platform please? MPU?

Also, the delay I was mentioning is the "ramp-up" delay after powering the PHY up. PHYs take some time before being fully functional (usually some us).

Regards,
Gatien

UthayaAuthor
Associate
August 29, 2025

Hi,

I am using samsung exynos v920 SOC  and i will try with ramp-up delay also.

 

UthayaAuthor
Associate
September 1, 2025

Hi,

I have tried with ramp-up delay but still facing same issue. i have added a delay in driver before probing but it didn't works.

Thanks

Uthaya M

UthayaAuthor
Associate
September 15, 2025

Hi 

Any suggestion from anyone, it would be helpful

Thanks & Regards

Uthaya M

UthayaAuthor
Associate
September 15, 2025

Hi 

Any suggestion from anyone, it would be helpful

Thanks & Regards

Uthaya M

Erwan SZYMANSKI
Technical Moderator
September 15, 2025

Hello @Uthaya ,
This forum is dedicated for STM32 product, and we cannot support other SoC outside from the ones provided by STMicroelectronics.

I advise you to contact the dedicated support for your product.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.