Skip to main content
Associate III
June 18, 2025
Question

the MAC address settings for the STM32MP257 network port

  • June 18, 2025
  • 1 reply
  • 312 views

Will the Linux driver for stm32mp257 automatically set the MAC address based on the chip UID?

Or do users need to set it themselves?

 

bugman_0-1750225931932.pngbugman_1-1750225965264.png

Why is the MAC address printed using dmesg different from the hardware address obtained from the command?

Thank you, looking forward to your reply~

1 reply

Olivier GALLIEN
Technical Moderator
June 19, 2025

Hi @bugman ,

 

Can you specify if you are on ST or Custom board ? 

 

Thanks

 

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
bugmanAuthor
Associate III
June 20, 2025

I am using Myir STM32MP257 board