Skip to main content
Associate II
January 2, 2026
Question

The SPI on the STM32MP257F-DK board doesn't work after the device tree setup

  • January 2, 2026
  • 1 reply
  • 291 views

Hello Everyone

linux kernel version: 6.6.78

After configuring the device tree, I can see the SPI device /dev/spidev6.0 on the STM32MP257F-DK board. However, when I run spidev_test[1], it returns the error message "Invalid argument."

I tried using an oscilloscope to measure the signals on the CLK, MOSI, and MISO pins separately, but no signals were detected.

Please give me some suggestions to help me fixed it. Thanks in advance.

//------------------------------------------------------------------------------------------------------

the SPI device tree setting as following:

Path:

~/STM32MPU-Ecosystem-v6.6/Developer-Package/BSP/sources/ostl-linux/linux-stm32mp-6.6.78-stm32mp-r2-r0/linux-6.6.78/arch/arm64/boot/dts/st/stm32mp257f-dk.dts

aliases {
 serial0 = &usart2;
 serial1 = &usart6;
 serial2 = &usart1;
 ethernet0 = &eth1;
 spi6 = &spi6;
 };

&spi6 { 
 pinctrl-names = "default", "sleep";
 pinctrl-0 = <&spi6_pins_a>;
 pinctrl-1 = <&spi6_sleep_pins_a>;
 status = "okay";

 spidev@0{
 compatible = "rohm,dh2228fv";
 reg = <0>;
 spi-max-frequency = <10000000>;
 };
};

 

reference:

1.How to use SPI from Linux userland with spidev, https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev.

                               

1 reply

Erwan SZYMANSKI
Technical Moderator
January 5, 2026

Hello @LeonSu ,
Are you sure you used properly the tool command by using the --device argument ?

If yes, can you share a bit more information about boot logs, and command logs ? 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.