Skip to main content
Associate
October 4, 2024
Question

Trying to detect SMIs latency on STM32MP157D-DK1

  • October 4, 2024
  • 1 reply
  • 1250 views

Hey, I’m working with an STM32MP157D-DK1, I’m trying to trace for System Management Interrupts, to check how they affect the system.

The following attempt was made to detect the latency of SMIs occurring on the system:

 

# mount -t debugfs debugfs /sys/kernel/debug

# mount -t tracefs nodev /sys/kernel/tracing

# cd /sys/kernel/tracing

# cat hwlat_detector/window

1000000

# cat hwlat_detector/width

900000

# cat tracing_thresh

10

# cat tracing_max_latency

0

# cat tracing_cpumask

3

# cat hwlat_detector/mode

none [round-robin] per-cpu

# cat tracing_on

1

# cat current_tracer

nop

# echo hwlat > current_tracer

# sleep 1800

# cat trace

# tracer: hwlat

#

# entries-in-buffer/entries-written: 0/0   #P:2

#

#                            _-----=> irqs-off/BH-disabled

#                           / _----=> need-resched

#                          | / _---=> hardirq/softirq

#                          || / _--=> preempt-depth

#                          ||| / _-=> migrate-disable

#                          |||| / delay

#       TASK-PID CPU#  |||||  TIMESTAMP  FUNCTION

#          | |     |   ||||| |     |

 

 

After a half hour sleep, it’s unclear why `trace` remains empty, and no iterations are shown detecting latencies.

Does the system not have SMIs at all? Or is there something wrong with what I’m doing?

Kind regards

1 reply

Erwan SZYMANSKI
Technical Moderator
October 7, 2024

Hello @FredBarkins ,
You talk about SMI but it seems that System Management Interrupts are specific to x86 architecture, not ARM.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
October 7, 2024

Hey sir thank you for your response.

You are right. Please note that according to the hardware latency detector documentation :

 


The tracer hwlat_detector is a special purpose tracer that is used to detect large system latencies induced by the behavior of certain underlying hardware or firmware, independent of Linux itself. The code was developed originally to detect SMIs (System Management Interrupts) on x86 systems, however there is nothing x86 specific about this patchset.

From what I'm getting, the arm equivalent to SMIs are interrupts running in Secure Monitor Mode.

I'm assuming that the reasons that x86 processors need SMIs (temperature management, ...) are inevitably present on arm cores too.

 

 

@Erwan SZYMANSKI 

Erwan SZYMANSKI
Technical Moderator
October 11, 2024

@FredBarkins ,
What is the Yocto configuration you tried to set it up ? Did you activate all the Ftrace needed in your image ? https://wiki.st.com/stm32mpu/wiki/Ftrace

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.