Skip to main content
Visitor II
March 11, 2024
Question

Wie kann man onewire auf dem STM32MP135 mit python nutzen?

  • March 11, 2024
  • 2 replies
  • 1030 views

I want to read a temperature sensor DS18B20 with onewire with the STM32MP135 in Python?
Does anyone know how to do this best?
I've already tried installing the onwire library from python, but that fails. I don't want to program it in C.

I'm new here, so I hope I've classified my problem correctly.

greetings

This topic has been closed for replies.

2 replies

PatrickF
Technical Moderator
March 12, 2024

Hi @birnnehi 

 

I succeeded to use DS18B20 with STM32MP157F-DK2 with the following setup

Connect sensor on:

  • CN2 pin 8 and pin 10 shorted together (USART3_TX and USART3_RX): sensor data (usually yellow wire)
  • CN2 pin 6 (VSS) : sensor ground (usually black wire)
  • CN2 pin 4 (+5V): sensor supply (usually red wire)

install PyDigiTemp python module

Boot the board using "stm32mp157f-dk2-a7-examples" device tree (option 2 in U-Boot when prompted).
This define USART3 as ttySTM1 on pins listed above.

If needed to confirm the tty port used on your system, please have a look to https://wiki.st.com/stm32mpu/wiki/Trace_and_debug_scenario_-_UART_issue#Checking_the_UART_probe

 

Then such kind of python code should work:

 

from digitemp.master import UART_Adapter
from digitemp.device import TemperatureSensor

sensor = TemperatureSensor(UART_Adapter('/dev/ttySTM1'))
temperature = sensor.get_temperature()

 

Regards

 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Uwe Bonnes
Chief
March 12, 2024

If the MP1 runs linux, there is also owfs, the one-wire-filesystem.