SPC5 Controller is Heating and not connecting with debugger. Hi,
We are using an SPC5 microcontroller for a motor controller application. All of a sudden, we weren't able to connect with our motor controller board, which runs on the SPC5 controller, and we also found that it was getting heated up to 36 °C.
and while checking, we found something short in the "VDD_HV_IO0" pin, and we have checked by removing all the decoupling capacitors too. Now, should I consider that the controller went off, or are there any other ways to fix or debug this issue?