SPC570s-DISP board: FlexCAN sends bad frames independent of CAN parameters Hello,I have similar problem with the SP570S-DISP board as described here:https://community.st.com/s/question/0D50X0000ArRejNSQS/spc570-can-outputs-bad-frame-independent-of-frame-parametersMy Configuration: 250KBaud, 16Tq, Sample-point=75%, XOSC 40MHz, CAN_clk 40 MHz, V_ext=12V/VDD_HV_IO=5V, Vector VN1610+CANoe running, 120 Ohm on both sides, ID=0x135, Data={0xAA, 0x55, 0x00, 0x00, 0xAA, 0x55, 0x00, 0x00} DLC=8. Clock settings:/* Setting the system dividers to their final values.*/
/*
* b0 : DE = 0b1 enable divider
* b9-15 : DIV (Divider is DIV + 1)
*/
/* System clock 0 divider */
MC_CGM.SC_DC0.R = 0x80000000UL;
/* System clock 1 divider */
MC_CGM.SC_DC1.R = 0x80010000UL;
/* System clock 2 disabled */
MC_CGM.SC_DC2.R = 0UL;
/* Pit clock divider 5 */
MC_CGM.AC0_DC0.R = 0x80040000UL;
/* SAR ADC clock divider 25 */
MC_CGM.AC0_DC1.R = 0x80180000UL;
/* CTU clock divider 25 */
MC_CGM.AC0_DC2.R = 0x80180000UL;
/* DSPI clock divider 4 */
MC_CGM.AC0_DC3.R = 0x80030