Are there any more detailed explanation regarding Teseo LIV3F software documentation UM2229 or binary image description UM2399? Hello, right now i am working with a STA8090 DevKit to test some things with the Teseo LIV3F. Unfortunatly, the software documentation is very inconsistent.For example in UM2399 Rev5 May 2020, there is the command$PSTMCFGCONST (page 151/376), which allows or disables different GNSS constellations.(Or UM2229, Rev 4 Dec 2019, page 86/239 and 87/239)Its described as every constellation is 1 decimal digit and can have following allowed values: Constellation disabledConstellation satellites only trackedSatellites constellation used in position evaluationBut what values? 0, 1, 2? Or 1, 2, 3?If i check a software command sheet from a different quectel module, which also uses the same command its listed as 0, 1, 2. If i check the software manual of Teseo VIC3DA, its listed a 1, 2, 3.However, if i type in a 9 or 13 like$PSTMCFGCONST,1,1,9,0,0 i still get a $PSTMCFGCONSTOK$PSTMCFGCONST,1,13,1,0,0 i still get a $PSTMCFGCONSTOKSo which value is now correct? 0, 1, 2 or 1, 2, 3 and why does the modu