Skip to main content
CTack.2
Associate
October 27, 2021
Solved

Help identifying quad OP Amp

  • October 27, 2021
  • 2 replies
  • 1725 views

0693W00000FDiFkQAL.jpgSee picture above for exact markings. No markings on the bottom of the IC.

Battery powered device (low voltage)

Markings:

ST (e3) 7B589

VA1814

PHL 423

Alternate version has similar markings. Maybe just a date code change?

ST (e3) 7B474

VA1814

PHL 423

This topic has been closed for replies.
Best answer by Peter BENSCH

Well, it's already published, just not where you expected it to be. As already stated, it is instead labelled on the box/packaging in which it is delivered.

Anyway - yes, I'm 100% sure VA1814 is the marking for TSZ124IPT.

Regards

/Peter

2 replies

Tesla DeLorean
Guru
October 27, 2021

My money is an ST second-source/equivalent to the LT1814

https://www.analog.com/media/en/technical-documentation/data-sheets/18134fa.pdf

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Peter BENSCH
Technical Moderator
October 28, 2021

@Community member​ is not completely right, it is the TSZ124IPT with marking VA1814.

Regards

/Peter

<edit>moved from Discontinued Devices to OPAMPs, because it is an active device</edit>

Tesla DeLorean
Guru
October 28, 2021

I can't be right all the time, but it helps significantly if the markings match what's in the documentation, and the documentation with the markings is spidered by Google.

If your web-devs are searching for productive tasks not involving just changing/fiddling the look/feel of the web portal, might I suggest some part#/marking search index that can help narrow parts from the past/present, along with suggested ordering numbers, or replacement/substitute parts. Bonus points for lead time information, estimated EOL date and 10-20-30 year availability status.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..