Soft AP does not work with the Cube example for B-L475E-IOT01A with ISM43362 There seems to be a bug when activating a Soft Access Point for the B-L475E-IOT01A MB1297D. The problem is either in the Wi-Fi module's firmware or in the es_wifi drivers in STM32Cube_FW_L4_V1.11.0 and STM32CubeExpansion_Cloud_AWS_V1.2.1. The es_wifi drivers expects a "[AP ]" reply from the module when the 'A0' command is sent. No reply is received and the ES_WIFI_ActivateAP will time out. Even though the module does not reply, the Soft AP starts correctly and the web server is able to configure a network.Only after a network is configured, the module will reply with the "[AP ]" message. Full output example:> [AP ] SSID: Soft AP network MAC: XX:XX:XX:XX:XX:XX ,11,192.168.10.1[WEB SVR] Server started>[SOMA][AP DHCP] Assigned XX:XX:XX:XX:XX:XX has 192.168.10.100[EOMA][JOIN ] Actual Wifi network,192.168.2.157,0,0OKSTM32L4 Discovery kit IoT node (B-L475E-IOT01A MB1297D) with ISM43362. Tested with these firmware versions:IS