I'm trying to recover some bricked STA8089FGBD's I have a significant number of bricked STA8089's, literally 100's, and I'm trying to find out why.The devices won't respond, VOL2 is lower than it should be (1.2V), the RF chain is dead (low supply voltage), and there seems to be no response to the serial port, at any bit rate. What do I need to do to recover to factory reset status. In an ideal world I'd like to get the CDB values out, but right now just recovering would be a good start. These are naked devices, no micro present, so any config / boot has to be serial / handshake based.