Teseo-liv3f after standby mode, no GPS signal anymore I am doing a GPS tracking project. I want to turn the GPS into standby mode or Enable Periodic Mode. I am doing the code in the Arduino IDEFor standby modeI use the following code to set the GPS into standby mode. MicroNMEA::sendSentence(gps,"$PSTMFORCESTANDBY,00010");Can I use any code to wake the GPS up in software way?I try the following code:MicroNMEA::sendSentence(gps,"$PSTMFORCESTANDBY,00010");delay(5000);MicroNMEA::sendSentence(gps, "$PSTMSRR");However, the GPS received no signal anymore.For Enable Periodic ModeI used the code MicroNMEA::sendSentence(gps, "$PSTMLOWPOWERONOFF,1,0,0,0,0,0,0,3,100,0,1,1,15,180");But this makes no any change while reading the output from serial monitor.Can anyone help give me a hint?Thank you!