Hello, I'm trying to transmit and receive via DMA UART on SPC58EC-DISP. On the other side there is a STM32L432KC: the SPC transmit to STM32 which receives the message, but the message transmitted to SPC by the STM32 is not received. I post the code #include "components.h"#include "serial_lld_cfg.h"void sddmatxcb(SerialDriver *sdp) { (void)sdp; pal_lld_togglepad(PORT_F, PF_LED2);}void sddmarxcb(SerialDriver *sdp) { (void)sdp; pal_lld_togglepad(PORT_F, PF_LED1);}/* * Application entry point. */int main(void) {uint8_t message= 3; /* Initialization of all the imported components in the order specified in the application wizard. The function is generated automatically.*/ componentsInit(); /* Enable Interrupts */ irqIsrEnable(); /* * Activates the serial driver 1 using the driver default configuration. */ sd_lld_start(&SD1, &serial_config_sddmacfg); /* Application main loop.*/ for ( ; ; ) {(void)sd_lld_write(&SD1,&message,1); osalThreadDelayMilliseconds(500); }}