Skip to main content
Dariush.Tsh
Associate III
December 6, 2021
Solved

SPC563M64L5 and SPC560P50L5 microcontrollers pin compatible

  • December 6, 2021
  • 1 reply
  • 840 views

Are the SPC563M64L5 and SPC560P50L5 microcontrollers pin compatible?

I mean, can two microcontrollers be assembled instead of each other?

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    There is only one common housing variant for both SPC: the LQFP144. If you look at both datasheets, you can immediately see that the SPC560P50L5 and SPC563M64L5 do not have any pin match, so they are definitely not pin-compatible.

    Regards

    /Peter

    1 reply

    Peter BENSCH
    Peter BENSCHBest answer
    Technical Moderator
    December 6, 2021

    There is only one common housing variant for both SPC: the LQFP144. If you look at both datasheets, you can immediately see that the SPC560P50L5 and SPC563M64L5 do not have any pin match, so they are definitely not pin-compatible.

    Regards

    /Peter

    Dariush.Tsh
    Associate III
    December 6, 2021

    OK, Tkanks...