Skip to main content
APANT.11
Visitor II
October 17, 2021
Solved

Hi, I am considering SPC58EC70E3F000X microcontroller in a design. 1. Can RTL8201F ethernet PHY from Realtek be used with SPC58EC70E3F000X microcontroller? 3. Does SPC58ECx/SPC584Cx has necessary libraries for Realtek Ethernet PHY ICs.

  • October 17, 2021
  • 1 reply
  • 814 views

..

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello Apant ,

    1) Yes ,

    10 and 100, Mbps data transfer rates with the following PHY interfaces:

    – IEEE 802.3-compliant MII interface to communicate with an external Fast Ethernet PHY

    – RMII interface to communicate with an external Fast Ethernet PHY  (ok for RTL8201F)

    2) In discovery board we are using CI Ethernet

    DP83848YB/NOPB

    We have no library on this IC.

    you have to create it.

    anyway , you can refer to the application :

    SPC58ECxx_RLA Network Ping Test Application for Discovery

    (Network component as example)

    Best Regards

    Erwan

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    December 2, 2021

    Hello Apant ,

    1) Yes ,

    10 and 100, Mbps data transfer rates with the following PHY interfaces:

    – IEEE 802.3-compliant MII interface to communicate with an external Fast Ethernet PHY

    – RMII interface to communicate with an external Fast Ethernet PHY  (ok for RTL8201F)

    2) In discovery board we are using CI Ethernet

    DP83848YB/NOPB

    We have no library on this IC.

    you have to create it.

    anyway , you can refer to the application :

    SPC58ECxx_RLA Network Ping Test Application for Discovery

    (Network component as example)

    Best Regards

    Erwan