Skip to main content
Larsa
Associate II
September 9, 2021
Question

SPC5 and using SPC572L we have problem with DPLL channel 16 - SPC5_GTM_DPLL_ACTION_ID_15 not working

  • September 9, 2021
  • 1 reply
  • 728 views

Our SPC572L application are using both MCS1 & MCS2 connected to DPLL and ATOM it works well on all 16 channels except the last one: channel 16 "SPC5_GTM_DPLL_ACTION_ID_15" if we change to ch17 "SPC5_GTM_DPLL_ACTION_ID_16" it runns fine but we need to use all 24 channels soon with the SPC572K device.

0693W00000Dmh8QQAR.jpg0693W00000Dmh8aQAB.jpg 

Is there a known workaround?

/Lars

    This topic has been closed for replies.

    1 reply

    ECAST.1
    Visitor II
    December 9, 2021

    Hello,

    Errata sheet are available on web-site:

    https://www.st.com/en/automotive-microcontrollers/spc572l64f2.html#documentation

    Some work around in the DPLL area, one of them could be useful for your issue.

    Regards,

    Emanuele