Flash Erase for SPC58NG84E7 is not working Hello,I am working on the bootloader, trying to flash only 256 bytes. So, before flashing, erasing the block 0xFF0000. There is already some data in this block. But erase is not happenin, even if FlashErase() returns 0 and FlashCheckStatus() also gives opResult=0. Also when I check memory, it still shows the same data and not erased.Following below steps to get flash block erased-#define LOWBLOCKSELECT 0x00000100U#define MIDBLOCKSELECT 0x00000000U#define HIGHBLOCKSELECT 0x00000000U/* Unlock the requested block for Erase operation */
nLargeBlockSelect.firstLargeBlockSelect = 0;
nLargeBlockSelect.secondLargeBlockSelect = 0;
SetLock(&FLSHM_ssdConfig, C55_BLOCK_LOW, UNLOCK_ALL_BLOCKS);
irqIsrDisable();
/* Erase the requested block */
Return_Val = FlashErase(&FLSHM_ssdConfig, C55_ERASE_MAIN, LOWBLOCKSELECT, MIDBLOCKSELECT, HIGHBLOCKSELECT, nLargeBlockSelect);
if(Return_Val == C55_OK)
{
while(C55_INPROGRESS == FlashCheckStatus(&FLSHM_ssdConfig,
C55_MODE_