0-10V(IP) dc to 0-3.3V(OP) dc analogue linear conversion circuit?
i want to convert 0-10V in to 0-3.3V linearly for analogue input of STM32 MCU so for this application any op-amp circuit which can done this?
i want to convert 0-10V in to 0-3.3V linearly for analogue input of STM32 MCU so for this application any op-amp circuit which can done this?
It depends on what you want to do with the output voltage: should it be measured or is it used for further processing with an internal comparator or opamp?
If it is to be measured: does it necessarily have to be converted to 3.3V, or can you also accept a lower output voltage?
To stay with the measurement: both have advantages and disadvantages:
Let's assume for the sake of simplicity that you want to measure the signal converted from 10V to 3.3V. Then you can, for example, reduce the 10V to 3.3V with a voltage divider 67:10 (e.g. 68k+33k or a better optimized ratio), then buffer it with a Unity Gain Buffer Amplifier as described here in Wikipedia, fig 3, and then connect it to the ADC input.
If the opamp is supplied by VDD=3.3V, you have to make sure that it is a RRIO amplifier, i.e. rail-to-rail input and output, like e.g. TSZ121 or TZ181. Of course you can also use other types with a larger offset, but don't forget that the offset is an error in the output signal.
Good luck!
Regards
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.