Skip to main content
CMayh.1
Associate
May 24, 2023
Question

BU508AW do you have an equivalent

  • May 24, 2023
  • 3 replies
  • 1502 views

..

    This topic has been closed for replies.

    3 replies

    Peter BENSCH
    Technical Moderator
    May 24, 2023

    Welcome, @CMayh.1​, to the community!

    The BU508AW is only available in the semi-insulated TO-247 and is still in production.

    However, it was developed for CRT TV at the time and the number of such projects has now shrunk drastically, so there is no reason to develop a comparable or better alternative. The BU508AW is thus the only npn BJT that STMicroelectronics has on offer in this package and with at least this VCES.

    Does it answer your question?

    Regards

    /Peter

    CMayh.1
    CMayh.1Author
    Associate
    June 8, 2023

    Thanks for getting back to me and yes it does answer my question, but are any available anywhere to purchase. I've tried RS and Farnell but they have no stock and none expected till November. I need six ASAP.

    Regards

    Chas

    Peter BENSCH
    Technical Moderator
    June 8, 2023

    I am very sorry to hear this, but the community is intended only for technical discussions that may be of interest also to other users at a later date. Availability is always temporary and must please and can only be clarified with the preferred or local distributor.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Good luck!

    /Peter

    AJens.5
    Visitor II
    June 8, 2023

    I don't know sorry.