Can STA309A at a fixed frequency of MCLK(XTI) 256 * Fs to give out a PWM with a frequency of 384 kHz?
Good day!
I want to use STA309A.
I want to signal MCLK (XTI) 256*Fs, bicki to signal 64*Fs.
What frequency of PWM will I get, 384 kHz or 256 kHz?
Real example
Fs = 32 kHz
MCLK (XTI) = 256 * Fs = 8192 kHz
BICKI = 64 * Fs = 2048 kHz
What is the frequency of the PWM output work?
I need a fixed frequency of 384 kHz.
Can STA309A at a fixed frequency of MCLK(XTI) 256 * Fs to give out a PWM with a frequency of 384 kHz?
Thanks.
With respect, Valery.