Skip to main content
trym1994
Visitor II
September 22, 2016
Question

Choosing the right amplifier

  • September 22, 2016
  • 0 replies
  • 492 views
Posted on September 22, 2016 at 15:22

I'm planning to make a speaker system, and need the right amplifier ic. The input have to be I2S and the amp is going to power four 8 ohms drivers with 50W max. Should I go with a single ic to power all four drivers or maybe a single one for each channel? Any tips or recs would be great!

#audio-amplifiers
This topic has been closed for replies.