How can I use differential audio input at TDA7292?
Hi, I'm trying to design hifi amplifier using TDA7292 refering its datasheet.
I read the datasheet of TDA7292, and I have some following questions :
- How can I use differential audio input at TDA7292? Is it okay to connect amplifier's IN1- and IN2- pin to differential audio source's L- and R- pin instead of connecting those amp pins to GND?
- With a single supply circuit, is it okay to supply single +48V 2A power to TDA7292? In TDA7292's electrical absolute maximum ratings, it the maximum DC supply voltage of TDA7292 is +-35V. But what I'm trying to design is single supply circuit. I wonder if it would be overloaded.
- Is there are any disadvantage using 'For Single supply' circuit instead of using 'For Dual rail supply' circuit?
- I found what I assume to be an error in the Figure22 diagram on page 17 in the datasheet. Pin 2 of the TDA7292 is OUT1 and pin 10 is IN1-, but in Figure 22 they are reversed. It seems to me that this is an error, am I right?
I'm newbie in circuit design, so please understand me if there are any sound like dumb question.
Thank you! :grinning_face: