Skip to main content
nmagniez
Visitor II
February 7, 2014
Question

I've installed the APWorkbench suite but I'm getting the following message when launching the application: ''APWorkbench I/O warning: No FTDI driver found, APWLink communication will be disabled…..''. Can you please provide more explanation about?

  • February 7, 2014
  • 5 replies
  • 1082 views
Posted on February 07, 2014 at 10:08

I've installed the APWorkbench suite but I'm getting the following message when launching the application: 'APWorkbench I/O warning: No FTDI driver found, APWLink communication will be disabled…..'. Can you please provide more explanation about?

    This topic has been closed for replies.

    5 replies

    Marco VENERI
    ST Employee
    February 7, 2014
    Posted on February 07, 2014 at 10:21

    The

    http://www.st.com/web/en/catalog/tools/PF253187

    is used to communicate with Sound Terminal evaluation kits and requires a third-party driver to operate correctly. Driver is available from

    http://www.ftdichip.com/Drivers/D2XX.htm

    .

    Though FTDI driver is already included in the APWorkbench setup package its installation will be completed only once an actual APWLink I/F is connected to the PC, via USB. If this does not happen the communication with such I/F will be disabled.

    Note that APWorkbench can still be operated either in simulation mode (no communication with any actual IC/device) or through an

    http://www.st.com/web/en/catalog/tools/PF258331

    , if available. Also, STAudioHub interface is recommended for ST MEMS Microphone evaluation.

    miguelernandez
    Associate
    April 9, 2014
    Posted on April 09, 2014 at 11:48

    depends on your windows you maybe have to install the drivers manually, even if windows thinks the drivers are okay then apworkbench will not find them

    jthuot
    Visitor II
    July 14, 2014
    Posted on July 14, 2014 at 17:37

    Hi,

    I'm experiencing the same issue with the FTDI drivers.

    Any luck on that front?

    Thank you,

    Jonathan

    jthuot
    Visitor II
    July 15, 2014
    Posted on July 15, 2014 at 16:16

    I have installed the drivers manually under Win7(64) with APworkbench(64), still not found.

    Any suggestion on what to do next?

    Marco VENERI
    ST Employee
    July 18, 2014
    Posted on July 18, 2014 at 15:42

    Jonathan,

    Make sure to download and install the proper driver version for your OS (64 bits) from the FTDI site.

    Also, the driver installation will be completed only after an actual STAudioHub board will be plugged on the USB port.

    Marco