Skip to main content
Paul Beijer
Visitor II
November 28, 2017
Question

Input bias current TS3022

  • November 28, 2017
  • 1 reply
  • 536 views
Posted on November 28, 2017 at 12:11

Hello,

I have a question about the TS3022 dual comparators.

The datasheet states an input bias current of 300nA max. over full temperature range.

Compared to similar competitor parts this is almost two orders of magnitude higher.

I was wondering if this specification is correct or should it be pA i.s.o. nA?

Thank you,

Paul

--

    This topic has been closed for replies.

    1 reply

    Pierre SENNEQUIER
    ST Employee
    January 2, 2018
    Posted on January 02, 2018 at 10:42

    Dear Customer,

      The unit is correct. You can see the typical behavior of the IC fig 12. of the datasheet.

      Best Regards,

      P.