Skip to main content
HGros.1
Associate
August 4, 2020
Question

LDO40L - max. input voltage on PIN ENAB without demage on worst case

  • August 4, 2020
  • 3 replies
  • 761 views

LDO40L -> Enable PIN. Can I connect this pin directly to Uin to the Enabble-Pin or must I use a resistor (for example 10K for limiting Current input to the PIN Enab) to connct Enab to Uin for enable the chip?

    This topic has been closed for replies.

    3 replies

    Peter BENSCH
    Technical Moderator
    August 4, 2020

    The datasheet of the LDO40L allows the voltage VEN at the enable pin voltage to be in the range of -0.3V...VIN (see page 5, abs max ratings).

    So connecting EN to VIN is definitely allowed, no limiting resistor is necessary.

    Good luck!

    /Peter

    HGros.1
    HGros.1Author
    Associate
    August 7, 2020

    Thanks for your answer.

    On Page 14/ figure 13

    If there is an input voltage jump within 1µs, is the output voltage deviation really 2V?

    Thnks an best Regards

    Heiko

    Peter BENSCH
    Technical Moderator
    August 7, 2020

    Perhaps you are referring to page 14, fig. 30 instead of fig. 13?

    Then the transient at 10->15V, 1µs, Cout=2.2µF and Iout=1mA can be as high 2V, as the datasheet says. That is a typical behavior with ultra low quiescent current LDOs at low output currents and can be influenced with external circuitry.

    Best regards

    /Peter