Skip to main content
Pavel_47
Associate III
November 9, 2023
Solved

Powering multiple optical front-ends

  • November 9, 2023
  • 4 replies
  • 1536 views

Hello,

There are 8 optical front-ends on the board ... the front-ends based on TSV771 (or TSV772, TSV782, TSV791, TSV792).

Is it important to use one LDO per front-end or powering all 8 frontends by a single LDO will be also Ok ?

Thanks.

This topic has been closed for replies.
Best answer by Peter BENSCH

As I said, I don't know the circuit or the necessary parameters, but I assume that ferrite beads could be a bit scarce because their inductance is usually quite small. Perhaps a simulation or a test could be useful.

For the capacitors, MLCCs might be the best choice.

4 replies

Peter BENSCH
Technical Moderator
November 10, 2023

Even if the opamps are used as transimpedance amplifiers, separate LDOs are not necessarily an advantage because their PSRR and its frequency dependence play a major role and should also be taken into account. Without knowing your application in detail, it might make sense in your case to use a single LDO and separate the supply voltages of the individual opamps cleanly with LC filters and a carefully designed layout including GND.

Hope that helps?

Good luck!
/Peter

Pavel_47
Pavel_47Author
Associate III
November 10, 2023

Hi Peter

Thanks. Considering that the PSRR is quite high at low frequencies and damps at high frequencies, perhaps ferrite beads would be sufficient to separate the VDDs of OpAmps ?

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
November 10, 2023

As I said, I don't know the circuit or the necessary parameters, but I assume that ferrite beads could be a bit scarce because their inductance is usually quite small. Perhaps a simulation or a test could be useful.

For the capacitors, MLCCs might be the best choice.

Pavel_47
Pavel_47Author
Associate III
November 10, 2023

Ok, thanks Peter.