Skip to main content
Visitor II
May 23, 2024
Question

RHF1401 - Protection diodes for VIN and VINB

  • May 23, 2024
  • 2 replies
  • 1590 views

We use the RHF1401 in a space application. In front of the RHF1401 we have a single to differential buffer, which is susceptible for radiation transients. So it can occur, that the RHF1401 receives a transient with -1.3V to 5.55V at is inputs. The transient is present for 15us.

How much current can the protection diodes manage?

We have series resistors which reduce the current of the transient (10.5mA negative pulse, 74.5mA positive pulse).

 

Figure3.png

Best regards, Alessandro

This topic has been closed for replies.

2 replies

Muhammed Güler
Senior III
May 23, 2024

These diodes are there for ESD protection. Considering the non-repetitive nature of the ESD signal you should not waste power on them.
If the transient voltage does not come very often, the prototype will most likely work.
If I were you, I would prefer to use one or two extra elements instead of hoping that the "parameter not written in the datasheet" will not cause any problems.

Associate
October 20, 2024

For Schumann reasonnance a simple LP filter can do the job ^^^^ 

Otherwise do you consider TVS 6V and 2 just after connector? How could we plan EM surge power in space? Shouldnt one mount the highest power TVS available? 

Are you asking the power induced in space travelling propellers?

Maybe one Tesla, ESA or NASA design engineer can share insights.

For the Shumann reasonnance a simple low pass filter could be okay ^^^