STA326 power supply, programming sequence and output filter
The STA326 datasheet (DocID11531 Rev 9) is unclear on a couple of points, so:
* Does the STA326 output power level depend on the output stage supply voltage (VCC[12][AB] on pins 4,8,11,15),
or does it depend only on the digital signal chain (digital input signal and volume and effects settings) ?
The output clipping level will of course depend on the supply voltage, so obviously I'm talking about power levels below clipping :)
* What are the frequency limits of the XTI/CLK pin (pin 27) ?
* Is there a required or recommended sequence for changing the input signal format and/or frequency ?
In the CLK/XTI pin (pin 27) section on page 12 of the Datasheet, it says:
'Care must be taken to provide the device with the nominal system clock frequency;
over-clocking the device may result in anomalous operation, such as inability to communicate.'.
So, when switching between formats, e.g. 16-bit 44.1 kHz, 48, 96 or 192 kHz (24-bit),
in which order must these values and signals be changed:
* LR clock input (pin 31),* Bit clock input (pin 32),* XTI clock input (pin 27, also referred to CLK),* Bits 0-4 in Conf Reg A (MCS♯ and IR♯),* Bits 0-4 in Conf Reg B (SAI♯ and SAIFB) ?When switching signal family (44.1 vs. N*48 kHz), the XTI/CLK pin must be switched between e.g. 11.2896 MHz and 12.288 MHz.
Is that variation within the overclocking limit ?How will the STA326 react to a (short) removal of the XTI clock (while switching between oscillators) ?
What happens when the XTI clock and LR/BIT clocks don't match during the switchover
- should the input signal (LR+BIT clocks) maybe be stopped during the switch ?
* Are there any app notes available for the STA326, e.g. output filter component and board layout recommendations ?
I'm especially interested in recommendations about how to choose the output filter components.
Is there a BOM available for the Drum reference board (for inspiration, I'm interested in the output filter components only) ?
#sta326 #ddx