Skip to main content
Mohamed Jallouli_2
Associate
July 20, 2017
Question

Synchronous Slave SAI Sub-block Clock Source

  • July 20, 2017
  • 1 reply
  • 669 views
Posted on July 20, 2017 at 14:13

Hello Community,

Does the SAI sub-block clock source matter when it is in Synchronous Slave mode with the other sub-block? In other words, should the two sub-blocks have the same clock source?

Thank you.

    This topic has been closed for replies.

    1 reply

    bendkhilarwa
    Associate III
    September 23, 2017
    Posted on September 23, 2017 at 21:10

    Hello, 

    To use two block SAI working synchronously, you need to configure the first block as an asynchronous master and the other one as a synchronous slave. Then, The two blocks will share the FS ,BCLK and MCLK lines. And each one will have its own data line.