Skip to main content
Associate
October 22, 2024
Question

TDA7492E - analog input section.

  • October 22, 2024
  • 1 reply
  • 2022 views

Hello,

I have two questions regarding TDA7492E amp. 

1. What is the common voltage for audio inputs? 
2. What is the maximum usable voltage on audio inputs? I would like to increase amplitude by op-amps, not the amp gain. 

Thank you and best regards,
Przemek

This topic has been closed for replies.

1 reply

Peter BENSCH
Technical Moderator
October 22, 2024

Welcome @Przemex, to the community!

Both questions can be answered together: the permissible input voltage range is -0.3V...4.6V. If the range below 0V is ignored, the AC input voltage may therefore have a peak-peak of 4.6V, typically coupled via a capacitor.

Hope that helps?

Regards
/Peter

PrzemexAuthor
Associate
October 22, 2024

Hello and thank you Peter!

I was wondering about this value (4.6V) because value is in the absolute maximum ratings table - voltage which should not damage device permanently. I can only guess that the mid point (bias) is 1,65V (3,3/2) and to keep symetry and unclipped signal, 3.3 V is maximum. However as I mention - it's only guessing because there is no information about it in datasheet and I don't have PCB yet :)

All the best!
Przemek

Peter BENSCH
Technical Moderator
October 22, 2024

You asked about the highest voltage, which is indeed specified in the absolute max ratings. Of course, this value must not be exceeded under any circumstances, otherwise there is a risk of losing the warranty or even defects in the device.

If the output voltage of the previous device is 3.3V because of its supply voltage, your assumption is correct. However, you do not need to add a DC offset because this is done via the coupling capacitor.

Good luck!
/Peter