TS512 simple protection against over-voltage applied to output
We are using your TS512 with (+/-15V rails) as a low current (1mA), 10V voltage follower.
We have a test case where the output the TS512 is pulled to a 19V/100mA source for just 600us, and I am trying to assess whether this transient could internally damage Q29 or Q30 or anything else in the o amp (referring to TS512 schematics from datasheet, see also below).
My understanding is that during such transient the negative feedback would try to pull the output down to -15V to counter back that transient, hence Q29 would be cut-off and R13 would prevent the B-E junction from breakdown. On the other hand Q30, I think it would be almost fully "on", which would potentially create a differential voltage across R14 of 19-(-15)=34V. The question is:
1. Would the output still limit to 25mA so would R14 be safe -and by extension TS512- during those 600us)?
2. Is there any other considerations to take into account to assess the robustness of this part under this transitory?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.