Solved
TSV912IQ2T absolute maximum input voltage
The following are some questions related to the absolute maximum ratings of the TSV912IQ2T which are not clear from the datasheet.
- Can the voltage on the input pins (2,3,5 and 6) swing to values greater than VCC + 0.2V (for example 50V) if the current is limited assuming there is a clamping diode to the supply pin?
- In the datasheet, there is the statement " VCC - VIN must not exceed 6 V ". In the example mentioned, 3.3V (supply voltage) - 50V (on input) = -46.7V. It is assumed that this is ok since it does not exceed 6V. Is that correct?
- In case the answer to question 1 is Yes, what would be the current limit value ?