Skip to main content
TPres
Visitor II
April 8, 2019
Question

What is the ACPI HID for the ST TDA7802 amplifier?

  • April 8, 2019
  • 0 replies
  • 550 views

Hi, I'm writing a Linux audio driver for an Intel platform which requires an ACPI firmware node in order to enumerate the device. Other Intel drivers [0] use the i2c-ACPIHID:00 naming convention so I have followed this by setting the CID in my ACPI DSDT table to be "TDA7802". However, I am led to believe this is incorrect [1], and I should assign an official HID.

Do ST have an official ACPI HID for the TDA7802 amplifier? If so, what is it?

Many thanks,

Thomas

[0] https://elixir.bootlin.com/linux/latest/source/sound/soc/intel/boards/kbl_da7219_max98927.c#L27

[1] https://lkml.org/lkml/2019/3/25/839

    This topic has been closed for replies.