Skip to main content
pgregson1
Associate III
May 31, 2020
Question

where can I get detailed specifications on the LD39300 linear LSO regulator?

  • May 31, 2020
  • 0 replies
  • 674 views

I need detailed specifications of the LD39300 LDO linear regulator. Specifically, I need the tolerance on the Vref reference voltage. I also need the confidence interval for the min and max values in the data sheet. As an example, I presume that for the value of the dropout voltage under the test conditions stated, the "typical" column states the mean value of the dropout voltage. But to what does the "Max" value refer? Is this the mean + 1 sigma, mean + 2 sigma, or mean + 3 sigma? Equivalently, does this mean that the actual value of the dropout voltage will be less than the stated maximum for 84.13% of the parts (mean + 1 sigma), 97.72% of the parts 9mean + + 2sigma), or 99.87% of the parts (mean + 3sigma)? This is important for high yields during manufacturing.

Please let me know as soon as you can. My need for this information is urgent.

Best regards,

Peter

    This topic has been closed for replies.