AEK-POW-BMS63EN as a Master Board in the daisy chain
Hi,
I would like to check if STM AEK-POW-BMS63EN board can be used as a first board in the daisy chain with the setup where we have external MCU (for example STMF103RB) and AEK-COM-ISOSPI1?
In the datasheet you describe difference between 'Master' and 'Slave' in the following way:

and all your AEK-POW-BMS63EN comes with SPEIN pin pull-down via R20:

Can you please clarify if the usage of AEK-POW-BMS63EN in the single BMS setup with external MCU is even possible?
BR,
MaraLo