AutoDevKit Integration & Java VM Error – SPC5 Studio / SPC5-MCTK-01
Hi everyone,
I'm working on a university project involving vehicle lateral control using the SPC5-MCTK-01 board. I'm using SPC5 Studio and AutoDevKit, but I'm facing issues with the setup:
AutoDevKit installation via SPC5 Studio (Help → Install New Software) fails repeatedly.
Launching AutoDevKit directly results in:
"Error: Could not create the Java Virtual Machine. A fatal exception has occurred. Program will exit."
Tested on both Windows 10 and 11 – same issue.
I'd appreciate help with:
Correct integration of AutoDevKit into SPC5 Studio
Fixing the Java VM error
Tips or resources for using SPC5-MCTK-01 efficiently
Thanks in advance!
Best regards